Mouser Press Room
Mouser Facebook Mouser Twitter Mouser RSS Feed Mouser YouTube Channel Mouser Google+ Mouser LinkedIn Mouser Subscription Center Mouser Blog
Mouser Press Room
New Product Announcement

Würth Electronics' WE-EPLE USB 2.0 Jack with Integrated EMC Filter and ESD Protection Now at Mouser

January 26, 2015 - Mouser Electronics, Inc., the global authorized distributor with the newest semiconductors and electronic components, is now stocking the WE-EPLE USB 2.0 Jack with Integrated EMC Filter from Würth Electronics. Marketed as one of the industry's first integrated, high-speed USB 2.0 jacks that includes a combination EMI and ESD filter, the WE-EPLE provides up to 15kV of ESD protection and is fully compatible with standard THT USB 2.0 jacks. This jack offers developers a drop-in replacement for existing USB 2.0 connectors, reducing EMI noise while shrinking PCB size without a costly redesign.

The Würth Electronics WE-EPLE USB 2.0 Jack with Integrated EMC Filter, available from Mouser Electronics, is pad-compatible with conventional USB jacks, allowing overall design dimensions to stay the same. This enables developers to transform existing designs into EMC- compatible systems in very little time. The integrated EMC filter eliminates broadband interference on voltage and signal lines, and is almost invisible for the signal lines. Offering some of the best noise filtering, Würth has used its deep knowledge of magnetics to provide the WE-EPLE with all the necessary components to control noise, including a data line filters as well as a filter for VDD. For ESD protection, the WE-EPLE complies with most ESD specifications, including IEC61000-4-2, IEC61000-4-3, and IEC61000-4-5.

Other key benefits and features of Würth's WE-EPLE USB 2.0 Jack with Integrated EMC Filter include Vcc filter impedance above 100Ω in the 20MHz range; common-mode suppression at 240MHz far in excess of 250Ω; and ESD suppression at levels of 10V at 15kV pulses.

The Würth Electronics' WE-EPLE USB 2.0 Jack with Integrated EMC Filter is available today through Mouser Electronics as a single port, four-contact female connector, with phosphor bronze contacts and gold plating. The WE-EPLE has an operating temperature range of -40°C to +85°C, is UL 94 V-0 rated for flammability, and is well-suited for commercial and industrial USB applications.

To learn more, visit http://www.mouser.com/wurth-we-eple-usb-jack/.

With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 20 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

About Mouser
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 500 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 400,000 customers in 170 countries from its 492,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.

About Wurth Electronics
The Wurth Electronics EMC & Inductive Solutions unit manufactures inductors, transformers, and EMC-components for global customers. Their success is based on more availability, more service, more presence, and more knowledge to give their customers a "little bit more to make the big difference". Wurth Electronics product lines include inductors, common mode chokes, transformers, snap-on ferrite line chokes, ferrite beads, connectors and modular filtered jacks.

Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.



Further information, contact:
Kevin Hess, Mouser Electronics
Vice President Technical Marketing
(817) 804-3833
Kevin.Hess@mouser.com
For press inquiries, contact:
Kelly DeGarmo, Mouser Electronics
Corporate Communications Manager
(817) 804-7764
Kelly.DeGarmo@mouser.com
Back to Press Room