STMicroelectronics' STM32G0 Discovery Kit, Now at Mouser, Helps Designers Evaluate and Use USB Type-C and PD Functions
May 14, 2019 - Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now stocking the STM32G0 Discovery kit from STMicroelectronics (ST). The comprehensive kit, based on the STM32G0 USB Type-C and Power Delivery microcontroller, offers all required interfaces for connection and interoperability with USB Type-C devices. The versatile STM32G0 Discovery kit provides access to the USB-C port to check the status of power capabilities when connected to USB-C hosts including smartphones, computers, and USB-C docking stations.
ST's STM32G0 Discovery kit, available from Mouser Electronics, is based on an STM32G071RB microcontroller with an Arm® Cortex®-M0+ core, 32 Kbytes of RAM, and 128 Kbytes of flash memory. The handheld case integrates a four-way joystick with selection button plus a 1-inch 128 × 64 pixel OLED LCD module for ease of use. The device's on-board ST-LINK/V2-1 debugger/programmer offers USB enumeration capability, enabling intensive debugging and development.
The kit offers multiple board external connectors, including a USB Type-C plug cable, USB with micro-AB connector for ST-LINK, USB Type-C receptacle connector, and 8-pin user extension connector including SPI, ADC, USART and I²C communication signals. The board's internal connectors include USB Type-C test points for main signals and two 8-pin GPIOs free pins.
The kit has three bidirectional current and power monitors with I²C interface, enabling the measurement of VBUS, CC1 and CC2 protected and isolated lines, as well as an onboard DC/DC converter that sustains a power supply with VBUS ranging from 3 V to 20 V. The STM32G0 Discovery kit can be combined with the STM32CubeMonitor-UCPD to create a professional-grade Power Delivery analyzer.
To learn more, visit www.mouser.com/stmicroelectronics-stm32g0-discovery-kit.
With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 750 manufacturers. Mouser offers 25 support locations around the world to provide best-in-class customer service and ships globally to over 600,000 customers in more than 220 countries/territories from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com