ON Semiconductor's STK984-190-E Power Integrated Module for Driving BLDC Motors Now at Mouser
November 21, 2016 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the STK984-190-E Power Integrated Module (PIM) from ON Semiconductor. Optimized for driving three-phase brushless DC (BLDC) motors in automotive applications, the module's seven MOSFETs are mounted onto a direct bonded copper (DBC) substrate, resulting in a compact module with excellent thermal performance taking up only half of the board space used by an equivalent discrete solution.
ON Semiconductor's STK984-190-E Power Integrated Module, available from Mouser Electronics, contains six AEC-Q101 qualified 40V, 30A MOSFETs configured as a three-phase bridge with an additional 40V, 30A high-side reverse battery protection MOSFET. The module's DBC substrate reduces thermal resistance, which lowers the operating temperature of the MOSFETs and decreases power losses while increasing reliability due to a limited change in temperature during thermal cycling. Reliability is also improved by the isolation provided by the DBC substrate.
Designers can combine the STK984-190-E module with motor controllers to build high-efficiency BLDC solutions with best-in-class thermal performance, built-in diagnostics, and an ultra-small PCB that saves critical size and weight. The module is supported by the STK984-190-EGEVB evaluation board, and is suitable for use in 12V automotive electric motor drive applications with power ratings up to 300W, such as electric pumps, fans, and windscreen wipers.
To learn more, visit http://www.mouser.com/new/onsemiconductor/onsemi-stk984-190-e/.
With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 22 global support locations and stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 600 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 500,000 customers in 170 countries from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About ON Semiconductor
ON Semiconductor is a premier supplier of high-performance, energy-efficient silicon solutions for green electronics. ON Semiconductor's broad portfolio of power and signal management, logic, discrete and custom devices helps customers efficiently solve their design challenges in automotive, communications, computing, consumer, industrial, LED lighting, medical, military/aerospace and power applications.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com