Altera's Non-Volatile MAX 10 FPGA Evaluation Boards
Now in Stock at Mouser
November 3, 2014 - Mouser Electronics, Inc. is now shipping the MAX® 10 FPGA Evaluation Boards from Altera Corporation. These evaluation boards support test and development of the new Altera Non‑Volatile MAX 10 Field Programmable Gate Arrays (FPGAs) featuring integrated dual configuration flash memory, embedded RAM, embedded DSP, analog to digital converter blocks, and embedded processor support, all on one die.
The Altera MAX 10 FPGA Evaluation Boards, available from Mouser Electronics, provide developers with a cost-effective platform to program and test the Altera MAX 10 FPGAs. Features include full logic, I/O, and power evaluation, Arduino shield expansion, and a prototyping area. A JTAG header allows for easy test and debugging, while programmable user LEDs provide status feedback. The evaluation board comes with all necessary software and IP including the GUI-based Quartus® II FPGA design software with Analog Toolkit, DSP Builder, Nios® II Embedded Design Suite, and PowerPlay Early Power Estimator.
Dual configuration flash memory integrated in MAX 10 FPGAs allows the device to store two chip configurations in a single chip. MAX 10 FPGAs update safely and reliably by keeping a fallback image in Flash. The new MAX 10 FPGAs contain up to 50,000 logic elements (LE) and boasts advanced processing capabilities in a low‑cost, single chip programmable logic device. MAX 10 FPGAs are built on a 55nm embedded NOR flash process with embedded SRAM, and are available with up to 500 user‑programmable I/O pins.
MAX 10 FPGAs include integrated 12‑bit 1Msps analog-to-digital converters (ADCs) with up to 18 input channels. MAX 10 FPGAs also include additional processing capabilities such as the Nios II real‑time soft core embedded processor, as well as Digital Signal Processing (DSP) blocks. An external memory interface for DDR3 memory is available on selected devices. 128‑bit Advanced Encryption Standard (AES) design security helps protect programmed devices from being reverse-engineered.
To learn more, visit: http://www.mouser.com/new/altera/altera-max10-dev-tools/ .
With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 20 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser Electronics
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 500 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 400,000 customers in 170 countries from its 492,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About Altera Corporation
Altera Corporation is the pioneer of programmable logic solutions, enabling system and semiconductor companies to rapidly and cost effectively innovate, differentiate, and win in their markets. Altera offers FPGAs, SoC FPGAs, CPLDs, and ASICs in combination with software tools, intellectual property, embedded processors and customer support to provide high-value programmable solutions to customers worldwide.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Vice President Technical Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Corporate Communications Manager
(817) 804-7764
Kelly.DeGarmo@mouser.com