Filtros

Opciones de disponibilidad
Seleccionar Imagen Número de referencia Fabr. Descripción Hoja de datos Disponibilidad Precio (EUR) Filtre los resultados de la tabla por precio unitario basándose en su cantidad. Cant. RoHS
SparkFun Accesorios SparkFun Behold the Hydra! This USB power cable probably looks a lot like something you've hacked together before. We do it all the time because what is a computer if not a 5V power supply that happens to run software?The Hydra brings the 5V and GND lines f
7En existencias
Mín.: 1
Múlt.: 1

SparkFun Accesorios SparkFun This is a 10-pack of wires that are pre-terminated with an alligator clip on one end and a female header on the other. Alligator clips are a staple item for any workbench or makerspace and with these cables you will be able to easily incorporate tho 10En existencias
Mín.: 1
Múlt.: 1

SparkFun Accesorios SparkFun USB-C is fantastic. What makes this cable even better is that one of the features we love so much about USB-C has been replicated to the USB-A 2.0 plug! These cables have minor yet genius modifications that allow them to be plugged into their ports 4En existencias
Mín.: 1
Múlt.: 1

SparkFun Accesorios SparkFun USB-C is fantastic. What makes this cable even better is that one of the features we love so much about USB-C has been replicated to the USB-A 2.0 plug! These cables have minor yet genius modifications that allow them to be plugged into their ports 2En existencias
Mín.: 1
Múlt.: 1

SparkFun Accesorios SparkFun It's the end of the world and you need a button to press. This is it. A 100mm diameter (outside diameter) dome illuminated push button comes with an LED securing nut and a pre-installed long life horizontal microswitch. Button can also be adjusted 7En existencias
Mín.: 1
Múlt.: 1
SparkFun Accesorios SparkFun This a simple breakout board for the button pads. Each LED and button is brought out to the side connectors. The connectors are soldered to the back side of the PCB. We recommend trimming the connector leads on the button side as short as possible to 9En existencias
Mín.: 1
Múlt.: 1
SparkFun Accesorios SparkFun This is a 35mm concave momentary push button similar to the ones you find on arcade games. Simple screw in design. Perfect for mashing. This button has a great tactile 'clicky' feel.Features:Concave plunger designDurable nylon materialMicroswitch: m 12En existencias
Mín.: 1
Múlt.: 1
SparkFun Accesorios SparkFun This is a 35mm concave momentary push button similar to the ones you find on arcade games. Simple screw in design. Perfect for mashing. This button has a great tactile 'clicky' feel.Features:Concave plunger designDurable nylon materialMicroswitch: m 10En existencias
Mín.: 1
Múlt.: 1
SparkFun Accesorios SparkFun This is a 35mm concave momentary push button similar to the ones you find on arcade games. Simple screw in design. Perfect for mashing. This button has a great tactile 'clicky' feel.Features:Concave plunger designDurable nylon materialMicroswitch: m 68En existencias
Mín.: 1
Múlt.: 1
SparkFun Accesorios SparkFun This is a 35mm concave momentary push button similar to the ones you find on arcade games. Simple screw in design. Perfect for mashing. This button has a great tactile 'clicky' feel.Features:Concave plunger designDurable nylon materialMicroswitch: m 3En existencias
Mín.: 1
Múlt.: 1
SparkFun Accesorios SparkFun This is a 35mm concave momentary push button similar to the ones you find on arcade games. Simple screw in design. Perfect for mashing. This button has a great tactile 'clicky' feel.Features:Concave plunger designDurable nylon materialMicroswitch: m 10En existencias
Mín.: 1
Múlt.: 1
SparkFun Accesorios SparkFun This is a resistive analog joystick very similar to those found on the PSP1000. These compact joysticks are different in that they have a very interesting 'slide' feeling.For wiring this part if you look at the device from the bottom the pin out go 17En existencias
Mín.: 1
Múlt.: 1
SparkFun Accesorios SparkFun This plastic knob accepts a 6mm shaft and has a 15mm outer diameter. They simple press-fit onto a shaft. These are clear so that they can be used with our illuminated rotary encoders.Documents:Dimensional Drawing 13En existencias
143Fecha prevista: 04/09/2026
Mín.: 1
Múlt.: 1

SparkFun Accesorios SparkFun Ever hear of a thing called RGB? Red Green Blue? How about an RGB LED? These 5mm units have four pins: one for each color and a common anode. Use this one LED for three status indicators or pulse width modulate all three and get mixed colors!Note: 125En existencias
Mín.: 1
Múlt.: 1

SparkFun Accesorios SparkFun If you ever find yourself connecting handfuls of resistors to the ground bus of your breadboard you may consider these SIL-packaged resistors as a time-saving alternative. This Singe In-Line component is actually 5 individual 330 Ohm resistors that 17En existencias
Mín.: 1
Múlt.: 1
SparkFun Accesorios SparkFun Schottky diodes are known for their low forward voltage drop and a very fast switching action. This 1A 40V Schottky diode is ideal for use with motor drivers such as the L298N. 41En existencias
Mín.: 1
Múlt.: 1
SparkFun Accesorios SparkFun These color-changing LEDs take the work out of creating crazy flashy blinky... ness. Simply apply power and the LED will cycle through the RGB colorspace: no external controller necessary! These bright and festive LEDs make great decorations LED " 50En existencias
100Fecha prevista: 09/11/2026
Mín.: 1
Múlt.: 1
SparkFun Accesorios SparkFun LED - 5mm Cycling RGB (slow) 51En existencias
Mín.: 1
Múlt.: 1

SparkFun Accesorios SparkFun Do you need that extra push over the cliff? The Small sized GTE (Goes To Eleven) Knob can fit onto potentiometers with a 6mm wide shaft thanks to a brass insert with a set screw. Unfortunately this knob does not play well with 1/4" shafts (nobody li 35En existencias
Mín.: 1
Múlt.: 1
SparkFun Accesorios SparkFun These are bare non-addressable 1 meter long RGB LED strips that come packed with 60 5060 LEDs per meter. As these are bare LED strips that have no protective coating your project won't be water proof but there is access to each 5060 LED and each str 25En existencias
Mín.: 1
Múlt.: 1
SparkFun Accesorios SparkFun We know this looks like a lot of our other LEDs but it's not! This is a PTH Addressable RGB LED with a WS2812 control IC built right into the LED. This PTH version is incredibly similar to its SMD cousin except it is a lot simpler to solder into yo 29En existencias
Mín.: 1
Múlt.: 1
SparkFun Accesorios SparkFun Amphenol FCI Clinchr Conn. (2 POS, F) 32En existencias
Mín.: 1
Múlt.: 1

SparkFun Accesorios SparkFun The SparkFun Qwiic Dual Solid State Relay is a power delivery board that allows users to switch two AC loads from a low power microcontroller using the SparkFun Qwiic connect system. The board features two 25A/250VAC solid state relays that utilize t 1En existencias
Mín.: 1
Múlt.: 1
SparkFun Accesorios SparkFun This is a common MOSFET with very low on-resistance and a control voltage (aka gate voltage) that is compatible with any 3-5V microcontroller or mechanical switch. This allows you to control high-power devices with very low-power control mechanisms. 17En existencias
Mín.: 1
Múlt.: 1
SparkFun Accesorios SparkFun The name says it all on this one. An ATmega328 in DIP package pre-loaded with the Arduino Optiboot (Uno 16MHz) Bootloader. This will allow you to use Arduino code in your custom embedded project without having to use an actual Arduino board.To get t 95En existencias
Mín.: 1
Múlt.: 1